KIT-CRD-CIL17N-HM3 was originally designed in OrCAD/Allegro. The source file for the layout is "KIT-CRD-CIL17N-HM3 - OrCAD Layout (Source File)" --> "KIT-CRD-CIL17N-HM3_V1R0.brd". For users that prefer Altium, the source files were converted to an Altium PCB in the folder "KIT-CRD-CIL17N-HM3 - Altium Layout (Converted File)" --> "KIT-CRD-CIL17N-HM3_V1R0.PcbDoc". Note that the import process used the built-in Altium importer and has not been validated, but it is provided for user convenience.

Altium files generated 1/27/2026.